Technical FAQs

Ask a Question

What are the Schneider Electric Modbus cable part numbers?

Title
Schneider Electric Modbus cable
 
Issue
Schneider Electric Modbus cable part numbers
 
Product Line
Modbus cable
 
Environment
Modbus RS485
 
Cause
N/A
 
Resolution
The Schneider Electric Modbus cable we recommend is a (double shielded twisted pair RS 485 Modbus serial link, supplied without connector)
for 100 m - TSX CSA 100
for 200 m - TSX CSA 200
for 500 m - TSX CSA 500
Was this helpful?
What can we do to improve the information ?