Technical FAQs

Ask a Question

What are the new features in the 140NOE77101 which replaces the 140NOE77100 ethernet module?

The 140NOE77100 can be replaced by the 140NOE77101. The difference between these two modules are outlined below.

Was this helpful?
What can we do to improve the information ?