Technical FAQs

Ask a Question

What is the analog input impedance for the HMISCU6B5?

Analogue input range 

-10...+10 V or 0...10 V - resolution: 12 bits + sign, input impedance: >= 1 MOhm

0...20 mA/4...20 mA - resolution: 12 bits, input impedance: 250 Ohm (tolerance: +/- 1 %)

 

Was this helpful?
What can we do to improve the information ?