Technical FAQs

Ask a Question

MTBF for the M340 BMXNOM0200 Serial module

MTBF M340 BMXNOM0200 Mtbf 30° Continuous Mtbf 30° Intermittent Mtbf 60° Continuous Mtbf 60° Intermittent Mtbf 85° Continuous Mtbf 85° Intermittent Nb Cpt Missing Nb Cpt Missing * Qty Nb Cpt Total * Qty Ratio Nb Cpt Missing / Nb Cpt Total
BMXNOM0200 869049.078 701988.875 382831.244 394571.018 187814.272 221622.905 6 7 520 1.30%
Was this helpful?
What can we do to improve the information ?