Technical FAQs

Ask a Question

Am I required to use IIS security with Vijeo Designer Web Gate?

Issue:
Am I required to use IIS security with Vijeo Designer Web Gate?

Product Line:
Vijeo Designer

Environment:


Cause:


Resolution:
IIS is a component of Windows that turns the PC into a web server.  Turning ON or OFF the IIS security will not affect Vijeo Designer Web Gate as the web server is on the Magelis unit and not the PC.  It is not needed for Web Gate.

Even if you had the PC Runtime with Web Gate, IIS is still not needed as the Runtime is managing the Web Server.
Was this helpful?
What can we do to improve the information ?