Technical FAQs

Ask a Question

What are the Quantum CPU Copro and 140NOE771xx IO Scanner capabilities ?

Title
Quantum CPU Copro and 140NOE771xx IO Scanner functionality

Issue
Listing of Quantum CPU Copro and 140NOE771xx IO Scanner functionality
 
Product Line
quantum CPU and 140NOE771xx module
 
Environment
Unity Pro Software
 
Cause
N/A
 
Resolution
Below is listed the Quantum CPU Copro and 140NOE771xx IO Scanner functionality.
Max. No. of Devices 64: 140 NOE 771 00 (Version 2.2 or earlier)
Max. No. of Devices 128: 140 NOE 771 00 (Version 3.0 or later), 140 NOE 771 01, and 140 NOE 771 11 only
Max. No. of Devices 128: HE CPU 651 x0
Max. No. of Input Words 4000
Max. No. of Output Words 4000

Was this helpful?
What can we do to improve the information ?