Technical FAQs

Ask a Question

Is the Magelis XBTZG935 compatible with Windows 7?

Issue:
Is the Magelis XBTZG935 compatible with Windows 7?

Product Line:
Magelis XBTGC/GH/GK/GT, HMIGTO/STO/STU, Magelis iPC, Compact, Smart, Panel PC, Box PC

Environment:


Cause:


Resolution:
Yes, the XBTZG935 is compatible with Windows 7 32 and 64bit.
Was this helpful?
What can we do to improve the information ?