Technical FAQs

Ask a Question

Is there a ModbusTCP function code to force ON a discrete Input reference (%I) ?

Title
ModbusTCP protocol capabilities

Issue
Ability to force ON a discrete Input reference via the ModbusTCP protocol

Product Line
Quantum , M340 and M580
 
Environment
Unity Pro software
 
Cause
N/A
 
Resolution
 No, the standard ModbusTCP protocol can not force ON a discrete Input reference (%I). It can only read a discrete Input reference.

Was this helpful?
What can we do to improve the information ?