Technical FAQs

Ask a Question

What is the chemical/material make up of the HMIGTO gasket?

Issue:
What is the chemical/material make up of the HMIGTO gasket?

Product Line:
HMIGTO

Environment:


Cause:


Resolution:
The HMIGTO gasket is made of NBR( Nitrile Butadiene Rubber ).
Was this helpful?
What can we do to improve the information ?