Technical FAQs

Ask a Question

Why M218 doesn't stop according to the Deceleration value in (VBag)PTOMoveFast FB?

If you set "Compensation" to 0, when stop signal is triggered, it will always stop as the max deceleration of system.
Was this helpful?
What can we do to improve the information ?