Technical FAQs

Ask a Question

How do you determine what the default IP Address is of a new Unity Momentum?

Deriving a Default IP Address from a MAC Address

The processor derives its default IP address from its factory-assigned MAC address. The MAC address for the processor is displayed on the front of the module.
The default address is in the format 10.10.x.y, where x and y are derived from the last 2 octets of the MAC address. To determine the default IP address of a module, follow these steps:

NOTE: There are many resources for converting hex numbers to decimal numbers. For example, you can use the Windows calculator in scientific mode.

Was this helpful?
What can we do to improve the information ?