Technical FAQs

Ask a Question

In Vijeo Designer v5.0, why do I get the following web gate error "Could not start runtime. (Operation completed successfully)"

If running Vijeo Designer v5.0 in Windows 7, the error "Could not start runtime. (Operation completed successfully)" may occur due to the user account settings preventing certain programs or add-ons running on the users PC. Move the bar notification in the user account settings from always notify to never notify and re launch Internet Explorer and web gate and the error should go away.
Was this helpful?
What can we do to improve the information ?