Technical FAQs

Ask a Question

What is the part number for the parameter copy module for Lexium 17/15 series dirves?

Issue: Part number

Product Line: Lexium 17/15

Environment: None

Cause: Obsolescence


The part number for the paramter copy module used with Lexium 17/15 seroes drives is AM0PCM001V000. As of the time this document is being writtten, the module is still being shown as available on the MySE system.

A picture of the module is shown below.

Was this helpful?
What can we do to improve the information ?