Technical FAQs

Ask a Question

What are the Cutout Dimensions for the Magelis XBTN401 HMI Panel?

The cutout dimensions for the XBTN401 HMI is 119.4 (+/- 0.5) X 63 (+/- 0.4) mm.
Was this helpful?
What can we do to improve the information ?