Technical FAQs

Ask a Question

Can a relay failure for the VIP410 be wired to a physical contact?

Issue 
Want a contact to operate if the VIP410 has an internal fault.

Product Line 
VIP410

Environment 
Programming inputs and outputs.

Cause 
The device has no protection when an internal fault occurs.

Resolution 
Yes it is possible to wire the watchdog to a physical contact.

For custom operation mode information see article /en/faqs/content/?id=FA241103


 
Was this helpful?
What can we do to improve the information ?