Technical FAQs

Ask a Question

Error Installing ION Setup: IONSetup.exe is not a valid Win32 application.

A user is trying to install the latest version of ION Setup software on a Windows XP machine and runs into error shown below:

Product Line
ION Setup 3.0 (latest software revision)

A user is installing latest software revision of ION Setup (which is supported on 64 bit application) on windows XP machine which is 32 bit application.

ION Setup installation on windows XP machine

The latest software revision of ION Setup is a 64 bit application and is not supported on a windows XP machine (32 bit application) .
- The software revision of ION Setup for windows XP machine can be downloaded from this article. 
Was this helpful?
What can we do to improve the information ?