Technical FAQs

Ask a Question

In Unity Pro V8.1, Build error message: "error during the ARM assembler phase" on application using index of array.

Goals and symptoms
This problem can occur, when EF like DEC, INC have as operand an indexed element of array  and when an operation is done on the index:
Example:
DEC(tab_affectation_dispo[index-1]);

Fixes:
The workaround consists to do the operation on the index outside the EF.
Example:
index1:=index-1;
DEC(tab_affectation_dispo[index1]);

This problem will be fixed in Unity Pro V10

Was this helpful?
What can we do to improve the information ?