Technical FAQs

Ask a Question

How many HTTP connections are supported by the TSXETZ410/510 module?

The TSXETZ410/510 support a maximum of 16 HTTP connections. 1 connected Internet browser can open 2 HTTP connections. As a result, 8 Internet browsers can be connected to a TSXETZ module.

Was this helpful?
What can we do to improve the information ?