Technical FAQs

Ask a Question

How do I obtain the default IP address of the TSXETZ510 module?


The default Ethernet interface IP address for the TSXETZ510 module is calculated from it’s MAC address. The default IP address is  85.16.xx.yy, where xx and yy are the last two octets
of the MAC address converted from hex to decimal.
Example:
The module’s MAC address is (in hexadecimal): 00 80 F4 01 12 20. [12 hex = 18 dec] and [20 hex = 32 dec]
In this case the default IP address is (in decimal): 85.16.18.32
 
Was this helpful?
What can we do to improve the information ?