Technical FAQs

Ask a Question

Unity Pro V8.1 : Loss of Alias after modifying DTM

Goals and Symptoms
Modifying a DTM in an application with Unity Pro V8.1 can lead to losing all of the equipment Alias (not just the ones that are linked to the modified DTM) created for the application.

Fixes
Install the hotfix: UnityPro_V81_HF0282888R to fix the problem.
The hotfix is available on http://www.schneider-electric.com

Note: This hotfix will not recover the lost Alias.

Was this helpful?
What can we do to improve the information ?