Technical FAQs

Ask a Question

What is the Current measuring tolerance for an Easergy Flite 116

Issue
A user would like to know the current measuring accuracy for an Easergy Flite 116

Product Line
Easergy Flite 116

Environment
Product Specifications

Cause
None

Resolution
The current measuring tolerance for a Easergy Flite 116 is +/- 1% at full load. The minimal current change it is able to detect is 6 amps.

 
Was this helpful?
What can we do to improve the information ?