Technical FAQs

Ask a Question

How do you make global changes to variables in a section in Unity Pro?

There is a feature in Unity Pro that will allow you to make multiple and/or global variable changes. The feature is called Replace Variables... when you right-click on an item in your section. This feature comes in handy when you have multiple sections with the same logic but different variables. To use this feature you can right-click on a single block or you can highlight multiple blocks at once. When you right-click select Replace Variables... A screen will appear where you can search for a particular pattern in your variables and replace with another. For example you could changed all variables starting with P1 and change to P2. Note: This feature does not work when links between function blocks are selected.
Was this helpful?
What can we do to improve the information ?