Technical FAQs

Ask a Question

What is the Part Number for the Quantum 40 point I/O Terminal Strip?

There are two part numbers for the Quantum 40 point I/O Terminal Strips: 140XTS00100- Finger Safe 140XTS00200- Standard
Was this helpful?
What can we do to improve the information ?