Technical FAQs

Ask a Question

How do you change the project version of a Unity Pro project?

The default setting in Unity is to increment the project version by .1 after every build. To change this setting and to set your own project version, Right-Click on the Project folder in Project Browser. Select Properties, then select the Identification tab. Once the Identification tab is open deselect the Automatic Increment feature and manually adjust the project version.
Was this helpful?
What can we do to improve the information ?