Technical FAQs

Ask a Question

What is the maximum input voltage the Magelis S-Box PC can handle?

Issue:
What is the maximum input voltage the Magelis S-Box PC can handle?

Product Line:
Magelis S-Box, HMIBSU, HMIBSO

Environment:


Cause:


Resolution:
HMIBSU are rated for 12...24Vdc +/- 5%, therefore, 25.2Vdc is the maximum voltage input.

HMIBSO are rated for 9...36Vdc +/- 5%, therefore, 37.8Vdc is the maximum voltage input.
Was this helpful?
What can we do to improve the information ?