Technical FAQs

Ask a Question

Can I replace lock system on old SAREL S3000 enclosure ?

To replace the lock on the S3000 enclosure that is necessary to order the part number : NSYTHL1242EPLM.
In addition it's mandatory to take off the old cam in order to reuse it.
It's also recommended to take off the old plastic nut to reuse it.

In case when old plastic nut can't be took off it's necessary to order a new plastic nut by ordering the part number : NSYTK1.
In this product take off the plastic nut and to put to the bin the rest of components.

 
Was this helpful?
What can we do to improve the information ?