Technical FAQs

Ask a Question

PRINT_CHAR_QX and INPUT_CHAR_QX don't work anymore with a Unity V7 application, after I upgraded the BMXCRA (or replaced with a new one)

An evolution has been made in the BMXCRA's firmware, to increase it's robustness. This evolution is not compatible with the PRINT_CHAR_QX and INPUT_CHAR_QX functions provided with Unity V7
You can either
- migrate the application to Unity V8.x, or
- downgrade the BMXCRA to version 1.30
Was this helpful?
What can we do to improve the information ?