Technical FAQs

Ask a Question

Is there an Advantys RTD module that have more than 2 channels?

No. 2 channels is the maximum and it is the STBART0200.
Was this helpful?
What can we do to improve the information ?