Technical FAQs

Ask a Question

Does the XBTGC1100T have sink or source outputs?

Issue:
Does the XBTGC1100T have sink or source outputs?

Product Line:
XBTGC1100T

Environment:


Cause:


Resolution:
The outputs on the XBTGC1100T are source output only. 
 

 
Was this helpful?
What can we do to improve the information ?