Technical FAQs

Ask a Question

Profile Automation tool for PL SCADA 7.20 fails if run on computer where 7.10 was previously installed

Issue:
Profile Automation fails for PL SCADA 7.20

Product:
PL SCADA 7.2

Environment:
PL SCADA 7.10 previously installed and removed before PL SCADA 7.2 installed.

Cause:
Registry keys for the profile automation tool do not get removed when SCADA 7.1 is un-installed

Resolution:
*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system. Always backup the registry before making any changes.*
1) Open the Registry, Start -> Run -> Regedit
2) Search for Profile.Automation and profileAutomation
3) Replace any path that is pointing to the SCADA 7.1 folder with a path pointing to the SCADA 7.2 folder
Was this helpful?
What can we do to improve the information ?