Technical FAQs

Ask a Question

TCSESM083F1CS0 is on back order. Is there another part number that is comparable in specifications?

Issue:
TCSESM083F1CS0 is on back order. Is there another part number that is comparable in specifications?

Product Line:
Connexium

Environment:


Cause:


Resolution:
You can use part number TCSESM083F2CS0.  This Connexium switch has the same features at TCSESM083F1CS0 but only have 6 copper and 2 fiber ports.  While the TCSESM083F1CS0 has 7 copper and 1 fiber ports.
Was this helpful?
What can we do to improve the information ?