Technical FAQs

Ask a Question

PME / PME4DC / PME4HC 8.1 & 7.2 default reports that support hierarchy

Issue
A user would like to know the default report templates that support hierarchy configuration.

Product Line
Power Monitoring Expert 8.1 / 7.2
Power Monitoring Expert For Health Care 8.1 / 7.2
Power Monitoring Expert For Data Center 8.1 / 7.2

Environment
Web Applications
Reporter

Cause
Not all PME default report templates support hierarchy. Hence, a user would like a list of default report templates that support hierarchy.

Resolution
The list of default report templates that support hierarchy are:

PME 7.2 (All versions):
  • Multi Device Usage Report
  • Single Device Usage Report
  • Tabular Report
  • Trend Report
PME 8.1 (All versions):
  • Calendar Month Trend
  • Calendar Trend Week
  • Consumption Ranking Report
  • Energy Comparison Report
  • Energy Usage by TOU
  • Energy Usage
  • Data Export - Extended
  • Data Export - Standard
  • Tabular Report
  • Hourly Usage
  • Multi Device Usage
  • Multiple Trend
  • Single Device Usage
  • Trend Report
Was this helpful?
What can we do to improve the information ?