Technical FAQs

Ask a Question

Numeric Gauges in Web Diagrams Read Zero

Issue
Numeric gauges in the Web Diagrams show a zero reading on the dial, but have a value in the block. The same gauges operate as expected in Vista.

Product Line
Power Monitoring Expert (PME) 7.2.2

Environment
Web Diagrams
Vista

Cause
This issue was identified as a bug in the Web Diagrams feature and should only affect this specific version (PME 7.2.2). The issue is caused when the "resolution" of the numeric object is configured for 0.

Resolution
Modify the resolution of the object to be a nonzero number. To access the resolution, open the diagram in Vista, right-click on the object, and select the Display tab.

Was this helpful?
What can we do to improve the information ?