Technical FAQs

Ask a Question

What does Save variable VL24 to VL31 mean in the Equations Editor in SFT2841 for Sepam series 40

The “Save Variables VL24 to VL31” is a feature that gives the customer an option NOT to save the data in variables VL24 to VL31 in an event of Sepam auxiliary power outage. By default, VL1 to VL31 can save data during an outage, but if you select No on the “Save Variables VL24 to VL31”, variables VL24 to VL31 will not save the data during an outage.

AEDL3

Was this helpful?
What can we do to improve the information ?