Technical FAQs

Ask a Question

Can the Quantum I/O cards be hot swapped?

Yes. The Quantum I/O cards are hot swappable. The only ones that are not are the Power supplys  and CPU's.
Was this helpful?
What can we do to improve the information ?