Technical FAQs

Ask a Question

Does the BMXPRA0100 support the BMXEHC0800 high speed counter card?

Issue:
I can't select a BMXEHC0800 in my BMXPRA0100 rack.

Product Line:
M340

Environment:
M340 I/O

Cause:
Does the BMXPRA0100 support high speed counter cards?

Resolution:
No. The BMXPRA0100 only supports discrete and analog I/O cards. The BMXEHC0800 is not supported.
Was this helpful?
What can we do to improve the information ?