Technical FAQs

Ask a Question

Does the TSXETG100 support Modbus ASCII with NO parity or ODD parity?

Issue:
Can a TSXETG100 support Modbus ASCII with NO parity or ODD parity?
 
Product Line:
TSXETG100, EGX100SD
 
Environment:
N/A
 
Cause:
N/A
 
Resolution:
No. For the TSXETG100, when the selection of transmission mode is Modbus ASCII then the parity option is not changeable and it is set on EVEN parity by default as per product design.
Hence in this case we would recommend to change the parity setting of connecting device accordingly in order to match with communication configuration of ETG100 gateway module for serial communication.
Was this helpful?
What can we do to improve the information ?