Technical FAQs

Ask a Question

Will Quantum discrete input modules lose their "Active" indication upon loss of communication to an RIO drop?

 Unlike 800 series IO the Quantum discrete IO modules will continue to indicate "Active" even after communication to an RIO drop has been interrupted.
This condition will not adversely effect the operation of the Quantum IO or the application. The Quantum discrete output modules will extinguish their "Active"
indications upon losing communication between CRP and CRA.

 The Quantum IO will extinguish  "Active" indications when used in the local rack and the PLC leaves run mode.
Was this helpful?
What can we do to improve the information ?