Technical FAQs

Ask a Question

What are the operating altitude ranges of the Magelis XBTN/R/RT targets?

Issue:
What are the operating altitude ranges of the Magelis XBTN/R/RT targets?

Product Line:
XBTN/R/RT

Environment:


Cause:


Resolution:
The XBTN/R/RT will operate between 0-2000m at 55°C and between 2000-4000m but the temperature must not exceed 50°C.
Was this helpful?
What can we do to improve the information ?