Technical FAQs

Ask a Question

Do we offer a Magelis HMI that is Class 1 Div 2 with the operating temperature of 0-55 Degree C?

Issue:
Do we offer a Magelis HMI that is Class 1 Div 2 with the operating temperature of 0-55 Degree C?

Product Line:
Magelis XBTRT500/511

Environment:


Cause:


Resolution:
Yes, we have the Magelis XBTRT500/511 that are Class 1 Div 2 with operating temperature of 0-55 deg. C.  But the XBTRT5xx are semi-graphic text terminals.
Was this helpful?
What can we do to improve the information ?