Technical FAQs

Ask a Question

Can OFS, OPC Factory Server, run as a Services without logging into Windows?

Issue:
Can OFS run as a Services without logging into Windows?

Product Line:
OPC Factory Server

Environment:


Cause:


Resolution:
No, OFS can not run as a Services without logging in.  It is required that you log in to Windows to have OFS run as a Services.
Was this helpful?
What can we do to improve the information ?