Technical FAQs

Ask a Question

Do Lexium 32A and Lexium 32C support third party motors?

No, you can not use third party motors with Lexium 32A or Lexium 32C

Only Lexium 32M with the optional accessory encoder module support use of third party motors.
Type of encoders supported for third party motors with LXM32M are Resolver or Analog ( Hifa ) and the correct encoder module must be selected based on the motor encoder technology.

Was this helpful?
What can we do to improve the information ?