Technical FAQs

Ask a Question

How come the Momentary ON button is unlatching when button is pressed on the Magelis Panel PC, Box PC, or HMIGTW7354?

Issue:
How come the Momentary ON button is unlatching when button is pressed on the Magelis Panel PC, Box PC, or HMIGTW7354?

Product Line:
Panel PC, Box PC, HMIGTW7354

Environment:


Cause:


Resolution:
There is a conflict in the Touch Screen driver with the Vijeo Designer Runtime.  To resolve this issue you need to uncheck "Enable press and hold for right-clicking" from Control Panel -> Touch Screen -> Emulate Mouse Tab -> Click Settings... (See below screenshots)



Was this helpful?
What can we do to improve the information ?