Technical FAQs

Ask a Question

Vertical Lines Are Invisible After Upgrade To SPM/PME 7.x

Issue

After upgrading to SPM/PME 7.x, the vertical lines on the Vista diagrams seem to disappear. The objects still exist on the diagram, but the graphic of the line is invisible.

Product Line

SPM 7.0
SPM 7.0.1
PME 7.2
PME 7.2.1
PME 7.2.2

Environment

Vista
Web Diagrams

Cause
This issue only affects users using the "vertical_line.wmf" standard graphic in their diagrams.

Resolution

Users may switch to using the "vertical_line.bmp" file, or download the "vertical_line.wmf" file attached to this article and replace the existing one in the ..\Power Monitoring Expert\config\diagrams\images\WMF_symbols.
Was this helpful?
What can we do to improve the information ?