Technical FAQs

Ask a Question

How do I navigate the PM5000 register list?

Issue:
A first time user of the document containing PM5000 series registers may have difficulty finding what they need.
 
Product Line:
PM5000 series meters.
 
Environment:
Microsoft Excel.
 
Cause:
The register list is part of a MS Excel document that contains containing many different types of data, as opposed to a traditional PDF list that only shows register information. Below is a link to the register list:
FA234017
 
Resolution:
The various worksheets at the bottom of the MS Excel window can be navigated using arrow buttons on the left side of the worksheet list. Navigate to “Register List”. Then, take note of the horizontal scroll bar on the right side of the worksheet list. This scroll bar has to be scrolled to the left as far as possible.
 
This should make viewing the register list more straight forward. See screen capture below for how to find an example register for system frequency.


 
Was this helpful?
What can we do to improve the information ?