Technical FAQs

Ask a Question

Is SQL Reporting Services used in Power Monitoring Expert 7.2.x or greater?

Issue:
Is SQL Reporting Services used in Power Monitoring Expert 7.2.x or greater? Previous versions required the use of Reporting Services for the Web Reporting feature. 
 
Product Line:
Power Mointoring Expert (PME)
 
Environment:
SQL Server Reporting Services
 
Cause:
Previous versions of software (ION Enterprise 6.0, StruxureWare Power Monitoring 7.0.x) required the use of Reporting Services. 
 
Resolution:
SQL Reporting Services is no longer used for versions of Power Monitoring Expert 7.2.x or greater. The Installation Guide explains that Reporting Services is not required to be installed when installing SQL Server. 

If an existing system is upgraded in-place from ION Enterprise 6.0 or StruxurWare Power Monitoring 7.0.x, Reporting Services will still exist, but it will no longer be used. Once the system is upgraded to PME however, Reporting Services can be uninstalled from the system. 
Was this helpful?
What can we do to improve the information ?