Technical FAQs

Ask a Question

What is the Port for RuggedCOM RMC30 to be Used in PME or ION Setup?

Setup parameters for RuggedCOM RMC30 to be used in PME (including all previous versions/editions) or ION Setup.

Product Line
Serial to Ethernet server

Power Monitoring Expert, PME
Struxureware Power Monitoring, SPM
ION Enterprise
ION Setup

When a device is used as a gateway to a meter, a port number is required to be assigned in PME or ION Setup.

The default local port is 50000 which is setup in Raw Socket Protocol parameters; refer to page 129 of the User Guide (attached to this article).

Note that the IP Address of the gateway is setup in the same page.

Accessing the Rugged Operating System (ROS) in order to change the parameters can be done using a browser:
  • (default address; pages 26-27 of the User Guide)
  • username: admin
  • password: admin

Complete information for RuggedCOM RMC30 device and documentation:

*Warning:  Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Installation Guide can result in permanent damage to the device, severe injury or death.

Was this helpful?
What can we do to improve the information ?