Technical FAQs

Ask a Question

What is required to change the BMXP342030 to the BMXP3420302 ?

 In order to convert the BMXP342030 to the BMXP3420302 V2.50 you need to load two files.
These files have to be loaded in a specific order. The files are attached to this FAQ.

 Step 1: Using Unity Loader => V2.3,  load the file named BMX2030_to_20302_B.ldx
 Step 2: Using Unity Loader => V2.3,  load the file named BMXP3420302_V250.ldx
Was this helpful?
What can we do to improve the information ?