Technical FAQs

Ask a Question

Is there a quick and convenient method which can be used to test a MA-0185-100 for proper operation?

The easiest way to determine if the MA-0185-100 is having difficulties is to swap it out if you have an available spare. If no spare is available you can move the tap
to another position along the trunk line to see if the problem moves with the tap.

 Specialized test equipment does exist which would allow you to determine overall network health including cable, taps, splitters and topology.
This equipment would include the TDR (Time Domain Reflectometer), LMR/LMT (reciever/transmitter) and the dB Attenuation box.



R81517
Was this helpful?
What can we do to improve the information ?