Technical FAQs

Ask a Question

Can ModScan 32 be used to configure Momentum IO bases ?

No. The ModScan 32 application cannot configure Momentum IO bases. It can read and write register references using Modbus serial or Modbus TCP .
Was this helpful?
What can we do to improve the information ?